{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why does my H-Type Power Conditioner make a high pitched noise?
Issue:

Customer's device is emitting a high pitch hum or buzz.

Product Line:

APC H Type Power Conditioner, Line-R Automatic Voltage Regulator

Environment:

N/A

Cause:

Uninterruptible Power Supplies, Power Conditioners and Voltage Regulators are all power conversion devices. These devics all utilize electrical components such as transformers, coils and inductors in the process of manipulating input power, to provide adequately filtered output power to the attached devices. These components all use electromagnetism while converting utility power from AC to DC or while boosting/trimming low/high utility voltage. The magnetic flux generated by these components may fluctuate magnetic fields rapidly, causing the component to physically vibrate. This high frequency vibration can often manifest itself to the user as a high pitch whine or buzzing, depending upon the frequency itself. These frequency are most often outside of a human's normal range of hearing and are therefore rarely observed.

Resolution:

Unfortunately, there is no method of reducing this noise in the device once in service.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.