{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why does the voltage on Digital Multimeter read higher than the actual output voltage on the Altivar VFD?

Article available in these languages: Thai

Issue:
Digital Multimeter reads higher voltage in the output voltage from the Altivar VFD than the actual voltage.

Product Line:
ATV12, ATV312, ATV630, ATV930, S-Flex, E-Flex, Altivar Drives

Environment:
All

Cause:
NA

Resolution:
Normally, a True-RMS Digital multimeter (DMM) will read about 20 to 30% higher output voltage than what the actual Output voltage is. The reason is that a standard True-RMS DMM cannot reliably filter out the PWM(Pulse Width Modulation) output waveform and High Frequency noise from the VFD. A DMM with a Low Pass filter can fix this issue and can measure the output voltage more accurately.

Schneider Electric Egypt and North East Africa