Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
To commission a BMEAHI0810 card to be fault tolerant (FDR), the commissioning procedure requires that all three Ethernet ports of the M580 processor be commissioned, active and in the same subnet
Issue

- Disabling one or both processors DIO Ethernet ports ETH2 or ETH3 (in the Switch tab in the processors configuration screen) causes the BMEAHI0810 not to go into Run after a power cycle of the system.

- If both ETH2 or ETH3 ports are Enable, the AHI will go into Run after a power cycle.

Product Line

M580, BMEAHI0810

Resolution

On M580 CPUs model 20, all Ethernet ports including the backplane have to be enabled for the BMEAHI0810 to function properly.
On M580 CPUs model 40, the backplane has to be opened, but for the 3 ports on CPU front panel it requires only the one connected to PC (service port) to be opened during commission.  The other two ports can be disabled.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.