Welcome the the Schneider Electric French website.
It looks like you are located in the United States, would you like to change your location?
Traduisez en francais
Browse FAQs
What is the function of Sepam IEC 61850 level 1 ECI850?
Published date:
12 March 2021
The ECI850 connects Sepam series 20, Sepam series 40 and Sepam series 80 units to an Ethernet network using the IEC 61850 protocol. It acts as the interface between the Ethernet/IEC 61850 network and a Sepam RS485/Modbus network. 1 PRI surge arrester (cat. no. 16339) is supplied with the ECI850 to protect its power supply.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.