{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the distance between PDU mounting holes on the NetShelter SX accessory rails?
Issue:


Product Line:


Environment:
All versions and serial ranges.

Cause:


Resolution:

In the 42U cabinet
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25")

In the 45U cabinet
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25")

In the 48U cabinet
There are 6 sets of PDU mounting holes, all are spread by 7U (311mm 12.25")

Schneider Electric Egypt and North East Africa