Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EOTE - "Browse for Folder" Dialog only shows the "Desktop" folder.
Issue:
When trying to add a path on Operator Terminal Expert, in the "Browse to file" dialog nothing comes up except for the "Desktop" file.
Browse for folder dialog

Product Line:
Operator Terminal Expert, Windows 11 OS

Resolution:
This issue comes up when the OS of the PC is Windows 11 and there is a OneDrive account synced with the PC. You need to stop syncing your Desktop folder with OneDrive. Please follow the next steps to stop the synching:

Important: Before proceeding, copy the files in those special folders to another folder or external drive. Please don’t copy them anywhere under Desktop/Documents/Pictures. This is because disabling OneDrive backup for a folder erases the local copies of the files. Copying them to a different location beforehand will ensure that you don’t need to download them again from the OneDrive cloud.
1. Right-click the OneDrive icon in the Notification area and click Settings.
2. Select the Backup tab, and click Manage Backup.
3. In the Manage folder backup dialog, click on the Stop backup link for "Desktop"
4. Click Stop backup in the confirmation dialog that appears.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center