Our Brands

Item count in cart is 0 My Products My Documents

Select your location

Welcome to the Schneider Electric Website

Welcome to our website.

Solutions

An ICSS solution integrates the process control and safety system at all times autonomously, compared to the traditional approach of isolated control and safety systems. ICSS manages and regulates the production process by means of a Distributed Control System (DCS) and Safety Instrumented System (SIS) using proven Foxboro and Triconex systems as well as a Fire and Gas detection System (FGS) and High Integrity Pressure Protection System (HIPPS) commonly used in complex refinery and petrochemical processes.
Processes are monitored in the form of visual alarm logs and historical archives. Operators are given real-time information necessary to make proper corrective actions. Should any unwarranted process upset occur despite operator intervention, the affected process units will be shutdown automatically by the highly integrated SIS (safety integrated System) and brought to safe condition.

Benefits and Differentiation

> Agile response needed for changes in process inputs, operating conditions and ambient conditions
> Managing the data integration of several plants
> Ability to interface with servers, EPCs and process licensors

Highlighted Offer: EcoStruxure™ Foxboro DCS

EcoStruxure Foxboro DCS (an evolution of Foxboro Evo) is an innovative family of fault-tolerant, highly available control components, which consolidates critical information and elevates staff capabilities to ensure flawless, continuous plant operation. More capable than a traditional distributed control system (DCS) it enables strategic integration of the following industrial control system components: high availability control processor, powerful I/O, high performance HMI, cybersecurity protection, unified control and safety through integration with the industry-leading EcoStruxure Triconex safety systems and an intelligent interactive maintenance dashboard.

> Discover now
> Preserve your investment with future-proof technology so you can grow easily and affordably
> Protect the operational integrity of your business for safe, secure, reliable production
> Enjoy greater operational insight for faster, more accurate decisions that enable better performance

Highlighted Offer: FLEX Automation Project Execution Methodology

A methodology, based on decades of project execution excellence, to reduce project capital cost up to 30%, to manage schedule to take automation off the critical path and minimize risks removing most of change requests.

FLEX is an innovative approach that uses project data as it matures from the earliest design phase down to complete detailed project engineering. This results in different project milestones and a new execution approach

> Find out more
> Engineering Workbench
> Templates & Rules
> Virtualized Engineering
> SPI Integration
> Intelligent Enclosures
> Universal IO

Highlighted Offer: EcoStruxure™ Triconex Safety Instrumented Systems

Triconex is the only safety system with a proven track record in Safety and Critical Control, as demonstrated by its 30 years of experience in safety systems, in excess of 13,000 installed systems used today in safety and critical control worldwide.

> See more details
> Protect human and asset safety
> Comply with environmental and regulatory standards
> Meet and exceed production targets through maximum process uptime
> Supported by the large staff of TUV Certified
Functional Safety Engineers
> Patented fault tolerant Triple-Modular-Redundant(TMR) controller
> #1 market share leader in process safety

EcoStruxure™ Foxboro DCS Ignite Your Profit Engine

Learn how EcoStruxure Foxboro DCS helps consistently deliver measurable operation profitability improvement safely, enabling 100% ROI in less than a year.

Historian

Interlac

 

Gutor PxW

InTouch

Solutions

Manage and regulate the production process by means of Distributed Control System (DCS), Safety Instrumented System (SIS) using proven Triconex system , Fire and Gas detection System (FGS) and High Integrity Pressure Protection System (HIPPS) for complex petroleum refinery and petrochemical processes.
Monitor process by visual alarm logs and historical archives. Operators are given real-time information necessary to make proper corrective actions. Should any unwarranted process upset occur despite operator invention, the affected process units will be shutdown automatically by the highly integrated SIS (safety integrated System) and brought to safe condition

Benefits and Differentiation

> Seamless integration of the control and safety systems, resulting in more reliable plant operation
> Elimination of common mode failures that could trip the process
> Reduction in engineering effort by utilizing a common engineering workshop to configure both systems
> Reduced commissioning time

Highlighted Offer: Tricon CX

Tricon CX is the most powerful safety system from Triconex. Each Tricon CX controller is capable of handling 31 I/O racks, 186 I/O modules, and 5,900 physical I/Os. Up to 254 nodes can be networked in a single peer-to-peer network allowing in excess of 1,500,000 physical TMR I/Os to be managed.

> Discover now
> Built-in high integrity and availability
> Fault-tolerant operation
> High-capacity handling — in excess of 1 million I/O points
> Fast scan times (from 10 milliseconds)
Two men wearing hard hats talking on an oil rig

Brochure

Tricon CX. Superior protection for your people, your production and your profits.

Brochure

Prevent hazardous conditions from causing unsafe incidents.

Historian

Interlac

 

Gutor PxW

Solutions

Process & Power integrates the systems of Process, Safety, EMCS and iPMCC, all required in the O&G industry without gateways . Unified engineering tools, common HMI and asset manager are also incorporated to result in simplification for the end user and designer.
Foxboro EVO distributed control system and Triconex safety system create value for customers through ease of integration by facilitating them with seamless integration of intelligent control systems and providing dependability for maximum productivity in a safe, secure and a reliable ecosystem. The idea is to simplify complexities through an efficient platform with similar touch and feel which can interoperate and communicate effectively.

Benefits and Differentiation

> Seamless plant operations across DCS & EMCS
> Reduced engineering & commissioning time
> Site coordination simplified, smaller footprint
> Increased operator effectiveness
> Cost savings on Training

Highlighted Offer: Intelligent Power and Motor Control Center (iPMCC)

Type tested solution supporting smart device installation, application & system architecture, wiring recommendation, engineering guides and EMC compliance. Based on high dependability communication architectures.

> Discover now
> Reduce costs and lead time at construction phase
> Detailed Low Voltage energy & process data visibility – anywhere and anytime
> Data-driven Energy Efficiency with more detailed and accurate information
> Predictive Maintenance and proactive alarming with possibility of transmitting all alarms immediately to appropriate users
> Totally integrated solution Low voltage with energy and automation control

Highlighted Offer: EcoStruxure™ Foxboro DCS

EcoStruxure Foxboro DCS (an evolution of Foxboro Evo) is an innovative family of fault-tolerant, highly available control components, which consolidates critical information and elevates staff capabilities to ensure flawless, continuous plant operation. More capable than a traditional distributed control system (DCS) it enables strategic integration of the following industrial control system components: high availability control processor, powerful I/O, high performance HMI, cybersecurity protection, unified control and safety through integration with the industry-leading EcoStruxure Triconex safety systems and an intelligent interactive maintenance dashboard.

> Find out more
> Preserve your investment with future-proof technology so you can grow easily and affordably
> Protect the operational integrity of your business for safe, secure, reliable production
> Enjoy greater operational insight for faster, more accurate decisions that enable better performance

Foxboro DCS

Improve your operation profitability by mitigating risk to continuous production, empowering operations talent with insight and providing future-proof technology that enables your business to easily adapt to change.

Brochure

Integrated power and process management for effective project implementation and consistent plant operation.
Learn more

Interlac

 

Gutor PxW

InTouch

System Platform

Intelligence

Information Server

Simsci

Advanced Video Analytics & Security

Protection of mission critical assets, both from security surveillance and operational monitoring perspectives.
<!-- Start SmartBanner configuration --> <meta name="smartbanner:title" content="mySchneider"> <meta name="smartbanner:author" content="Schneider Electric SA"> <meta name="smartbanner:price" content="Free"> <meta name="smartbanner:price-suffix-apple" content=" - On the App Store"> <meta name="smartbanner:price-suffix-google" content=" - Google Play"> <meta name="smartbanner:icon-apple" content="//lh3.googleusercontent.com/lAVirntKlp63vbntUZvOkMvZI8fE4rIoA5Lwif9M09VxzFhcWE21sTDYqJqOqIPqg4m4=w300-rw"> <meta name="smartbanner:icon-google" content="//lh3.googleusercontent.com/lAVirntKlp63vbntUZvOkMvZI8fE4rIoA5Lwif9M09VxzFhcWE21sTDYqJqOqIPqg4m4=w300-rw"> <meta name="smartbanner:button" content="VIEW"> <meta name="smartbanner:button-url-apple" content="http://m.onelink.me/e5bff3e5"> <meta name="smartbanner:button-url-google" content="https://app.appsflyer.com/com.schneider.qrcode.tocase?pid=Web&c=Smart_app_bannerEG"> <meta name="smartbanner:enabled-platforms" content="android"> <!-- End SmartBanner configuration --> <link rel="stylesheet" href="[PublicationUrl]/assets-re1/css/smartbanner.min.css" /> <script type="text/javascript" src="[PublicationUrl]/assets-re1/js/smartbanner.min.js"></script>
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
Start your sales inquiry online and an expert will connect with you.

Chat

Do you have questions or need assistance? We’re here to help!