Browse FAQs

E-FLEX enclosed drive - After the main breaker got tripped, the drive has no display and won't run.

Published date: 19 August 2020

Issue:  
Why the main breaker in an E-FLEX  tripped, the drive has no display and won't run?

Product line:
Altivar ATV61

Environment:
All models, all serial numbers 

Cause:
DC bus is only reading 14 VDC on PA + to PC -      

Resolution:
Checked Line voltage L1 L2 L3 they are all good  490 vac phase to phase. DC bus on PA to PC was only 14 VDC, but it should be 680 VDC. 
Suspect  a issue with the input diode circuit, soft charge board, power board and or DC bus capacitors. Power down and do an static check on the input side of the drive PA to L1 L2 L2 and PC to L1 L2 L3.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.