{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

A customer's main power supply is 380Vac, and his motor nominal voltage is 440Vac. Could the motor output voltage also reache to 440Vac at nominal spe...

Goals and Symptoms

A customer's main power supply is 380Vac, and his motor nominal voltage is 440Vac. Could the motor output voltage also reache to 440Vac at nominal speed if "Uns" is set to 440? Is there any problem of this setting?

Causes and Fixes

It's not possible for the inverter to provide a output voltage upper to the main supply ( lower possible ). So in your case you can try to supply the motor under 380 V, you will obtain instability but depend to the application.


Legacy KB System (APS) Data: RESL157202 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.