Browse FAQs

Is there a Telefast solution with premade cables available for the BMXAMO0410 ?

Published date: 10 April 2020

The ABE7CPA21 Telefast block is available with one of the following premade cables:
BMXFCA150 - 1.5 m
BMXFCA300 - 3 m
BMXFCA500 - 5 m

Each cable has one 20-way terminal block on one end and one 25-way D-sub connector on the other end for sub-base (ABE7CPA21).


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.