{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

How to enable auto scroll in DM6000 and PM1000 series?

There are 3 modes of auto scroll.

1.) Scrolling within the level.
Keep pressing the down key for at least 3 seconds, the parameter name will be scrolled within the level (Refer QSG) and when the key is released meter will display “Auto” for a moment, which means the auto scrolling is enabled.
2.) Scrolling within the page.
Keep pressing the UP key for at least 3 seconds, the parameter name will be scrolled within the page and when the key is released meter will display “Auto” for a moment, which means the auto scrolling is enabled. Here also the auto scroll is similar to the earlier one (down key). But within the page.
3.) TURBO Parameters (Favourite pages earlier) auto scroll
Keep pressing the TURBO key (Earlier called FAVOURITE key) for at least 3 seconds, the parameter name will be scrolled as per the FAVOURITE page sequence (ref QSG) and when the key is released “Auto” will be displayed for a moment, which means the auto scroll of the TURBO parameters is enabled. It will start scrolling through the all the TURBO parameters.

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.