{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Too Many Pages" error in ION Enterprise Vista client

Goals and Symptoms

 

Upon opening up a Vista diagram, following error message pops up multiple times:

================
INFORMATION
----------------------
Too many pages
<OK>
===============

Causes and Fixes

 

 
The Too many pages error is due to the use of large numbers of Data Log viewers in one user diagram. Each log viewer in a diagram file triggers the creation of a "Log Plotter" page, and the pointers of all the created pages are stored in a global array which has a limit of 60. When opening a diagram that includes more than 60 data log viewers, the limit of this array is reached and the error dialog is displayed.

The workaround is to reduce the number of Data Log viewers contained in a single diagram.

This is problem in all ION Enterprise releases up to and including ION Enterprise 6.0 Service Pack 1.

There is a hot fix available for this problem for ION Enterprise 6.0 SP1 only. Contact Technical Support if it is required.



Public
Last Updated: May 20, 2011
All content © 1992-2011 Schneider Electric
text
 

Legacy KB System (APS) Data: RESL200456 V2.0, Originally authored by DaMi on 11/10/2009, Last Edited by JaMc on 05/21/2011
Related ranges: ION Enterprise V6.0, ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0, ION Enterprise V4.5, ION Enterprise V4.0
Explore more
Explore more