Browse FAQs

Is it possible to see the fault current and fault type after tripping in Compact NSX with Micrologic 5 and Micrologic 6.

Published date: 05 September 2020

Yes, it is possible to see the fault current and fault type after tripping in Compact NSX with Micrologic 5 and Micrologic 6. The external 24V DC must be provided to Micrologics. After Fault trip, the type of fault (Ir, Isd, Ii, Ig), the phase concerned and the interrupted current will be displayed by the Micrologic 5 and 6.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.