Browse FAQs

Can TeSys LR97D or TeSys LT47 be used with external CTs?

Published date: 12 March 2021

  • LR97D & LT47 can operate with the external CTs. 
  • The value to be set in the LRD97 or LT47 is to be chosen based upon the output of the CT. 
  • CTs can be chosen from the CT offer in the PowerLogic Catalogue (check attached file)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.