{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What's the part# of the programming cable for the TM221 controller?

Issue:
Part# of the programming cable for the TM221 controller

Product Line:
TM221

Resolution:
The programming cable that goes between the TM221 controller and a PC is BMXXCAUSBH018 (USB to mini-USB cable)

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.