Browse FAQs

How do I troubleshoot an ATV212 that has been running fine and suddenly displays an OC1 fault?

Published date: 13 September 2020

Issue:
ATV212 drive has been running for a while with no issues and suddenly displays an OC1 fault

Product Line:
All ATV212 drives

Environment:
All

Cause:
NA

Resolution:
OC1 is an overcurrent fault during acceleration. The motor is trying to pull more current than the drive can handle. Since the drive has been running fine for a while with no issues, chances are that the programming was done properly, and something has changed either on the load side (load is dragging-pulling more amps for some reason) or on the supply side (line voltage is dropping).  

Try these troubleshooting steps: 
1. Check for any new issues in the application. Typically ATV212 drives are used in fan applications. So check for obstructions in the fan (debris in the blades, worn out bearings, etc) 
2. Check for mechanical issues in the motor 
3. Measure line voltage to determine whether the proper voltage is being supplied to the drive and balanced phase-to-phase

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.