Browse FAQs

Can I determine the voltage for the SFlex drive given the part number?

Published date: 15 September 2020

Issue:
How will I determine the voltage for the SFlex drive given the part number?

Product Line:
ATV212 enclosed S-flex systems.

Environment:
All models, All serial numbers.

Cause:
Wants to know the voltage of Sflex drive through the part number

Resolution:
The ninth digit determines the type of voltage for the Sflex drive. 
For example: SFD212CG4YX07

Read from left to right
[SFD212] First six digits
[C] Seventh digit
[G] Eighth digit
[4] Ninth digit


2 = 208 Vac
3 = 230 Vac
4 = 460 Vac

The "4" on the Ninth digit indicates that this is a 460 Vac

Check the Catalog number description in the Sflex manual.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.