Browse FAQs

BMXCRA312x0 and the BMECRA312x0 remote adapters 'Custom RPI' parameters settings does not work.

Published date: 30 March 2021

Custom RPI settings for the BMXCRA312x0 or BMECRA312x0 remote adapters do not work when using Unity V13.1, CE V14.0, or CE V14.1.    

For example, if the RPI is set to 31ms in the following configuration,


The RPI does not display the change in the DTM.


The issue is resolved in:
  • Control Expert V15.0
  • Control Expert V14.1 using HotFix1 (HF1)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.