GYIK keresése
{"searchBar":{"inputPlaceholder":"Keresés kulcsszó alapján, vagy kérdés feltevése","searchBtn":"Keresés","error":"Adja meg a keresendő kulcsszót"}}
What is the right substitution for SE RCD, if the customer wants to change PFIM-U types from Eaton?
For applications with three phase VSDs, Schneider can only offer B SI type .
The type S (Selective) Medium sensitivity devices (100 to 1000 mA sensitivity), include a minimum time delay of 40 ms (depends on the level of leakage current ).
So specifically, we can offer as in attached image.
SI type has 8/20 µs impulse withstand, 5 kA conforming to EN/IEC 61008-1.
We do not have a 100 mA sensitive B SI devices.
{"support":{"yesButton":"Igen","noButton":"Nem","feedback":{"title":"Miben fejlődhetnénk?"},"submitButton":"Küldés","successMessage":"Köszönjük visszajelzését","title":"Hasznos volt az információ?","feedbackPercentLabel":"ember hasznosnak találta","captcha":{"error":"Jelölje be a négyzetet"}}}