Browse FAQs

Is a padlocking device available for the GV2MC** type enclosures?

Published date: 28 February 2020

Issue:
Padlocking device for GV2MC Enclosures

Product Line:
TeSys GV2 Manual Starters and Protectors

Environment:
n/a

Resolution:
Yes, use the GV2V01. When this is padlocked, the starter is automatically in and will remain in the OFF position.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.