Browse FAQs

What are the dimensions for the ATS01N230LY and ATS01N244LY?

Published date: 21 August 2018

Issue:
What are the dimensions for the ATS01N230LY and ATS01N244LY?

Product Line:
Altistart 01

Environment:
All

Cause:
N/A

Resolution:
Both units have the same dimensions:
4.96 (126 mm) inches deep
5.75 (146 mm) inches tall
7.09 (180 mm) inches wide

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.