Browse FAQs

What are the techniques to optimize the memory usage of Vijeo Designer project.

Published date: 30 July 2018

The following are helpful guidelines to optimize the memory usage of Vijeo Designer project.

 

1. Delete unused variables
2. Use indirect addresses and delete duplicate panels or popup window panels
3. Reduce the size of large bitmaps
4. Use the exact same image object for bitmaps
5. Use Text Block Display for large text files
6. Reduce the number of alarms stored in memory
7. Optimize memory usage in scripts
8. Reduce the color depth of bitmaps

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.