Browse FAQs

What is an ATV31****378?

Published date: 13 August 2018

Issue:  
What is an What is an ATV31****378?
 
Product Line: 
ATV31
 
Environment:
N/A

 
Cause:   N/A
 
Resolution:   
This is a special drive for Buhler Company. The 378 suffix indicates that logic input LI6 can be used as a 24vdc pulsed speed reference. Would need to obtain a replacement from Buhler Company. May also be identified as S378 suffix.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.