Browse FAQs

Which are the latest GSD file revisions for ProfibusDP communication board of the Altivar 71 Drive.

Published date: 29 July 2018

The latest GSD File revisions required for ProfibusDP communication board of the Altivar 71 Drive are as follows:

 1. The correct revision of GSD File for Profibus Card version V1.1IE01 is revision 3.
 
2. The correct revision of GSD File for Profibus card version V1.1IE03 is revision 5.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.