Browse FAQs

Which are the environmental conditions in which the Hoist Resistor of Altivar 71 Drive be used.

Published date: 08 July 2018

The environmental conditions applicable for the Altivar 71 Drive Hoisting Resistor usage are: 

1. Relative Humidity range from 5% to 93%, without condensation or dripping.
 
2. Air must be without corrosive gas, dust and condensation.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.