Browse FAQs

Can the ATV12 keypad be used with the ATV312 or ATV32 drives?

Published date: 11 June 2018

Issue:
Can the ATV12 keypad be used with the ATV312 or ATV32 drives?

Product Line:
Altivar ATV312 and ATV32

Environment:
All

Cause:
N/A

Resolution:
Yes. VW3A1006 can be used with ATV312/32 drives.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.