Browse FAQs

How do you wire up a 24vdc push pull encoder to the VW3A3407 encoder option card for the ATV71 drive?

Published date: 20 March 2020

Issue:
How do you wire up a 24vdc push pull encoder to the VW3A3407 encoder option card for the ATV71 drive?

Product Line:
ATV71 with VW3A3407

Environment:
All 

Cause:
Encoder wiring 

Resolution:
The pin outs may vary depending on the encoder type and connector type.

Basic setup is as follows:
A from the encoder goes to A on the encoder card
B from the encoder goes to B on the encoder card
A not and B not are tied together and jumper to 0V on the encoder card.
+24vdc goes to +V encoder card
0V goes to 0V on the encoder card


 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.