Browse FAQs

What can we do if we have OBF or OCF fault on ATV58 while we use the braking resistor ?

Published date: 03 April 2018

Issue:
What can we do if we have OBF or OCF fault on ATV58 while we use the breaking resistor ?
 
Product Line:
ATV58
 
Environment:
OBF or OCF 

Cause:
 n/a

Resolution:
OCF-Overcurrent Faut:
Recheck all the motor parameters.
Monitor the output current to see if it is drawing more than the FLA of the motor.

OBF-:Overbraking Fault:

The ObF fault occurs when the DC bus voltage spikes up over 840VDC.  If the drive is telling the motor to stop but the fan is being pushed by other fans, could be regenerating energy back onto the bus of the drive.  Have customer to monitor the DC bus voltage on the + and - terminals.
Measure the line voltage and compare to the displayed line voltage (Uln, in the display menu).
Measure the DC Bus voltage (Should be square root of 2 times the input line voltage).
Increase the DEC parameter (Adjustment menu).
Set the BrA parameter (drC menu) to yes. This allows the deceleration ramp to be automatically increased to avoid overbraking fault.  The BrA should be set to no, if using a braking resistor.
Check the Braking Resistor

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.