Browse FAQs

Is it possible to upload messages from the ESI06210 module, edit the messages, and download the modified file to the ESI06210?

Published date: 05 April 2018

Yes. Follow these steps if you want to use a text editor to modify the ESI messages.

ULOAD

1: Open a session of Hyperterminal.

2: Place the ESI module into configuration mode by
pressing the "reset button".

3: At the "CLI>" prompt, type "ASCII"

4: In Hyperterminal under the "Transfer" tab you'll find
a selection for "Capture Text". Select it.

5: Declare a file name and the path to where the
ULOAD will be stored and select "Start".

6: At the "ASCII>" prompt, type ULOAD.

7: You should now see a "txt" file in the directory
chosen in step 5 which contains the ULOAD.

***Very important!!!

Once you've completed the upload go back to the "Capture Text" selection and select "Stop".

If you don't the Capture Text utility Will continue to run.
This will prevent you from using the DLOAD option.


DLOAD

1: Open a session of Hyperterminal.

2: Place the ESI module into configuration mode by
pressing the "reset button".

3: At the "CLI>" prompt, type "ASCII"

4: At the ASCII> prompt type DLOAD
"YOUR FILE NAME"

5: In Hyperterminal under the "Transfer" tab you'll find
a selection for "Send Text File". Select it.

6: The file should now be downloaded to the ESI


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.