Browse FAQs

Which executive is required for a Momentum 171CCS76000 controller at PV:02?

Published date: 06 June 2018


A Momentum 171CCS76000 controller at PV:02 has a minimum executive of version 2.06.
The table below details the executives required for 984LL and IEC programming:
 

Programming Language Minimum Executive Required
984LL M1LLV206.bin
IEC -- Concept v2.1 B2.1 M1IV206B.bin
IEC -- Concept v2.2 SR2 M1V206C.bin
IEC -- Concept v2.5 SR2 M1IV206D.bin

Note: These executives can be downloaded from our website at www.modicon.com

Legacy KB System (APS) Data: RESL121736 V2.0, Originally authored by MiMa on 06/06/2013, Last Edited by DaSo on 06/06/2013
Related ranges: Modicon Momentum

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.