Browse FAQs

What does the letter R at the end of a Sy/Max part number mean?

Published date: 02 May 2018

The letter R indicates that the part has been repaired or refurbished at the factory and is not a new part.


Note: The Symax product line was made obsolete is 2015 and has limited support. It is recommended to upgrade to the M580 product line and you are able to keep the Symax I/O or can replace with the x80 I/O with the QWA adapters for more information contact your local Schneider Electric sales office. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.