Browse FAQs

How do I switch between 'Monitor mode' and 'Program mode' in the ProWORX NxT software?

Published date: 03 April 2018

There are two ways to switch between Monitor and Program mode in the ProWORX NxT software:
1. From the Network Editor Menu bar, click Edit and then Program Mode.
2. From the Status bar, located at the bottom of the ProWORX NxT screen the word 'Monitor' will be displayed. Clicking on this word will toggle it to 'Program'.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.