Browse FAQs

What replaces the 110CPU31101 controller?

Published date: 03 April 2018

The closest functional replacement for the 110CPU31101 is the 110CPU51201. There are several differences to consider between these units:

  • Both units have the same basic I/O; however the 110CPU51201 offers 2 additional 24 VDC high speed inputs
  • The 110CPU51201 has an onboard 24 VDC power supply (for the additional 2 24VDC inputs) whereas the 110CPU31101 does not have this feature
  • The 110CPU31101 utilizes a 8MHz CPU , whereas the 110CPU51201 utilizes a 16 MHz CPU, so throughput is faster with the 110CPU51201.
  • The 110CPU31101 has 512 words of data memory and 1024 words of program memory whereas the 110CPU51201 has 2048 words of data memory and 2048 words of program memory
  • The 110CPU51201 has a enhanced instruction set that also includes PID II and floating point math
  • The 110CPU51201 has two Modbus slave ports (whereas the 110CPU31101 only has one)
The program's configuration will need to be changed to reflect the new hardware installation.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.