Browse FAQs

How do I create a R_TRIG in Concept structured text?

Published date: 13 August 2018


In structured text it is sometimes possible to duplicate the function of a block already in the instruction set. This can be desirable to customers who have scan time concerns. Creating the function directly in the editor rather than calling the FFB from the instruction set will solve faster.

Below is the representation of a R_TRIG block from in a FBD section:

Below is an example of calling the R_TRIG FFB from a structured text section:

Below is an example of creating the R_TRIG functionality without calling the FFB; this example will solve fast than the two examples above:


Note: this FAQ was written with the Concept programming software but will also apply to users programming with Unity Pro.

Legacy KB System (APS) Data: RESL168477 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.