Browse FAQs

What is the difference between the Compact AS-BDAP-208 and the AS-BDAP-258 relay output modules?

Published date: 03 April 2018

The only difference between the two Compact relay output modules is that the AS-BDAP-258 module operates at extended temperatures.
Operating Temperature:
AS-BDAP-208.....0 to +60 degrees C
AS-BDAP-258.....-40 to +70 degrees C


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.