Browse FAQs

What are the differences between the Micro 110CPU61200 and 110CPU61203 controllers?

Published date: 18 February 2020

Issue
PLC differences

Product Line
Modicon Micro

Resolution
The Micro 110CPU61200 and 110CPU61203 controllers have the same specifications. The only difference are the output specs.
110CPU61200.....has 12 relay outputs
110CPU61203.....has 12 Triac FET outputs


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.