Browse FAQs

What impact does setting %MWi Reset on Cold Start have after a download of my application to the Quantum CPU?

Published date: 16 April 2018

If the %MWi Reset option is selected any %MW reference in the Data Editor which has an assigned value can expect that value to be transferred to the CPU on a Cold Start.
If the %MWi Reset option is de-selected all %MW values in the PLC will be initialized to zero, regardless of whether there are values in the Data Editor for the %MW references.. 


 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.