Browse FAQs

What is the replacement part number for the Quantum 140CPU53414A?

Published date: 25 June 2018

The replacement part number is the Quantum 140CPU53414B. As of 2015 the 140CPU53414B controllers are obsolete due to parts obsolescence and it is recommended to go to the Quantum Unity based hardware.

NOTE: The Quantum Unity based processors will be end of life on 12/31/18 and replaced with the M580 that is currently now being sold.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.