{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

ION Enterprise 6.0 - Client machines that do not meet minimum version requirements cannot be upgraded once the Primary has been upgraded.

Goals and Symptoms

One of the requirements to upgrade ION Enterprise Server or Client system from either v5.5 or v5.6 to v6.0, is to have Service Pack 2 (SP2) of the relevant version installed prior to the upgrade. Considering that, if an ION Enterprise Server is upgraded to v6.0 before its Client(s) are applied with SP2, this will lead to a failure in upgrading the Client(s) to v6.0. Furthermore, Client(s) will not be able to work with the Server due to a version difference, hence; itll be impossible to apply SP2 due this very same reason.

Causes and Fixes

: If the problem above manifests, modifying the registry key to bypass the Installer requirement would be the solution. Please note that all the changes should be made on the Client Computer. Prior to make changes, its recommended to create a back-up of the registry. To do so:<