Browse FAQs

Is there a tool that will allow logging of device data on Modbus TCP Ethernet networks?

Published date: 19 June 2018

Yes, Schneider Electric offers the Simple Modbus TCP Logger, 332SMTL0000 that can be
purchased online from http://eclipse.modicon.com/

text text
Simple Modbus TCP Logger is a simple yet powerful software tool that will enable
you to easily track and log data from Modbus TCP compatible devices. Now, you
can log data from PLCs, temperature APS_SENSORS, flow meters, or remote IO on Ethernet.
In fact, any device that communicates using the open Modbus TCP standard can
be logged with Simple Modbus TCP Logger. This low cost, user friendly, utility will
track and store data from up to 10 devices.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.