Browse FAQs

Why do I get an error code ( Invalid value in the length field of the control block ) 2003 Hex on my MBP_MSTR block in Unity Pro?

Published date: 05 April 2018


The most common reason for this error code is way the Control and Databuf elements were configured.

The Control pin must be configured as a array of Integers of at least 9 components long.
The Databuf pin must be configured as an array the length of the data that is to be read and/or written by the MBP_MSTR block.

In this example:
The MBP_MSTR is reading 20 registers from a local Modbus Plus slave PLC so a derived datatype was created Data_Storage_Type of length 0..19 or 20.
The Control type was created of type INT length 0..9 or 10.



Next create two variables one of each type and locate them to a %MW (4X) address.



Link these variables to the corresponding pins on the MBP_MSTR block, re-build the application, load the application to a controller, and the error code will be gone.


R-8117

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.