Browse FAQs

How to Connect to a MB+ network with Concept on a remote PC using a MBX Gateway?

Published date: 15 May 2018

MBX Driver Suite v6.0

Causes and Fixes

Note: For information on how to setup the MBX Gateway Client and Server see the resolution entitled "How to connect remotely to a MB+ network via TCP/IP using the MBX Gateway driver".
To Connect to a MB+ Network with Concept from a remote PC via the MBX Gateway you must chose the Adapter/Device number of the MBX Gateway Client in the Communication Setup.

First chose Connect from the Online menu.



Chose the Modbus Plus, the Device Number of the MBX Gateway Client, and then the address of the PLC on the Network.
Hit OK to connect to the PLC.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.