Browse FAQs

How to check and see which addresses have been used in a ProWORX NxT project?

Published date: 14 June 2018

Goals and Symptoms

To see which addresses have been used in a ProWORX NxT project.

Causes and Fixes

With your ProWORX NxT project open, click on Display then Used table. This will open the Address Used window. Click on the Rebuild Used button to update the addresses used.
Below are the different types of information you can display in the table:

Logic Only: When selected, the table displays information as follows:
x - Address used in logic.
u - Coil used in logic.
. - Unused address.
c - Coil duplicated in logic.

Traffic Cop: When selected, the table displays information as follows:
x - Address used in logic.
u - Coil used in logic.
. - Unused address.
T - Address used in the Traffic Cop and logic.
U - Address used in the Traffic Cop, in logic, and as an output coil.
t - Address only used in the Traffic Cop.

Peer Cop: When selected, the table displays information as follows:
u - Coil used in logic.
x - Address used in logic.
. - Unused address.
P - Address used in the Peer Cop and logic.
U - Address used in the Peer Cop, in logic, and as an output coil.
p - Address only used in the Peer Cop.

I/O Scanner: When selected, the table displays information as follows:
u - Coil used in logic.
x - Address used in logic.
. - Unused address.
D - Address used in the I/O Scanner and logic.
U - Address used in the I/O Scanner, in logic, and as an output coil.
d - Address only used in I/O Scanner.

All: When selected, the table displays information as follows:
x - Address used in logic.
u - Coil used in logic.
. - Unused address.
D - Address used in the I/O Scanner and logic.
d - Address only used in I/O Scanner.
P - Address used in the Peer Cop and logic.
p - Address only used in the Peer Cop.
T - Address used in the Traffic Cop and logic.
t - Address only used in the Traffic Cop.
U - Coil used in three or more different locations.
M - Address used in three or more different locations.

To view an address type, click the corresponding tab.....0xxxx, 1xxxx, 3xxxx or 4xxxx.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.