Browse FAQs

How to program an TCP/IP Address into an ECM-RM?

Published date: 20 January 2020

Product Line
ECM-RM
CM2000

Environment
ECMConfig

Resolution
Use an NR&D (SC-902) cable with a CAB108 wired to the same colors as indicated on the ECM-RM.

  1. Set the ECM-RM to Run mode. (By default this switch is in run mode)
  2. Set your computer to com port to 9600, even, 8, 1.
  3. Use the ECMConfig software.
  4. Type in the IP Address in the designated location
  5. Click Update
  6. Push the reset button on the ECM-RM
  7. Configuration Status will change from Brown to Green indicating that an IP Address has been set in the ECM-RM (This should only take a few seconds).


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.