Browse FAQs

How to set Clock in the FDM121 Display module of Compact NSX MCCB.

Published date: 27 February 2020

The date and time in the FDM121 display module of Compact NSX can be set either from the supervisor or from the Micrologic software utilities RSU and RCU or from PMC Modbus. It will automatically get synchronized between IFM module, FDM module, BSM module and the Micrologic.
 
Refer the attachment for the setting details and format of date and time.
 
Note: If the FDM121 module lost the power like MCCB gets open then the Clock get reset in FDM121 display module. To maintain the clock in FDM121 display module, external supply of 24V DC has to be provided.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.