Browse FAQs

How to connect the 4 Pole RCCB in 240V AC Single phase network.

Published date: 26 March 2019

To use the 4 Pole RCCB in 240V AC single phase network, connect the Neutral at N and Phase at terminal 1 of the RCCB.
 
Confirm the functionality of the RCCB with the help of the Test Push Button. The RCCB should trip when the Test Push Button is pressed.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.