Browse FAQs

How is the BMXART0414 or the BMXART0814 module wired for Millivolt measuring ?

Published date: 06 June 2018

Title

What terminals are used to connect a mV signal?

Issue

 

Product Line

Modicon M340

Environment

Unity Pro

Cause

 

 

 

Resolution

The mV signal is connected to the terminals labeled MS+ and MS- of the specific channel on the ART module.  These are the same terminals that a thermocouple would be wired too.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.