Technical FAQs

Ask a Question

Does the 140NOC78000 support the Unity MBP_MSTR operation code 15 ?

 

Title
140NOC78000 Unity MBP_MSTR operation code 15
 
Issue
Explain requirements for 140NOC78000 support of the Unity MBP_MSTR operation code 15 .
 
Product Line
Modicon Quantum.
 
Environment
Unity Programming software version 7.0 or greater
140NOC78000 firmware version 1.61 or higher
 
Resolution
Yes, the 140NOC78000 module supports the Unity MBP_MSTR operation code 15 when programmed with Unity 7.0 or higher and the firmware of the 140NOC78000 is at version 1.61 or higher .
Was this helpful?
What can we do to improve the information ?