Browse FAQs

Is there an isolated AC input module for the M340 PLC platform ?

Published date: 30 August 2018

Title

Does M340 have an isolated AC input module ?

Issue

 

Product Line

Modicon M340

Environment

 

Cause

 

Resolution

Yes, there is an isolated AC input module for the M340 PLC.  The part number is BMXDAI0814 and attached is documentation.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.