Browse FAQs

Do the Advantys STB EOS and BOS bus extension modules require bases?

Published date: 22 June 2018

Title

Are bases required for the Advantys STB end of segment and beginning of segment modules?

Issue

 

Product Line

Advantys STB

Environment

 

Cause

 

Resolution

Yes, each extension module requires a special IO base. The end of segment (EOS) module requires the STBXBA2400 IO base and the beginning of segment (BOS) module requires the STBXBA2300 IO base. The EOS module is installed at the end of each segment (except for the last segment on the island). The BOS module is installed at the beginning of each extension segment (except for the first segment on the island).


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.